Solar energy

Main image

Securing the future with solar energy

Solar energy is the future. Every year, the sun provides us with around 10,000 times the global energy requirements of mankind. The tremendous potential of the largest energy source can be nowhere near exploited, but we can all benefit from it – with photovoltaic systems that make efficient use of the energy. Since the increasing system voltage of modern photovoltaic systems requires equally more powerful cables and components, LAPP has established itself as a leading provider of innovative and high-quality solutions in the field of solar cables and connectors.

Industries-benefits-solar-eng

Products for PV systems

L3-Solar-energy-kuvitus

Product list

Get an insight into our product portfolio for photovoltaic systems, and discover the wide range of options that we have to offer.

Solar cables

Standards: EN 50618 / HD 60364-5-52 / IEC 62930 / H1Z2Z2-K / UL 854

Find solar cables online

 

Low-voltage cables

Copper

  • NYY
  • (N)YY
  • RV-k
  • RZ1-k
  • CU-XLPE-SWA-PVC
  • CU-XLPE-LSZH-SWA-LSZH

Aluminum

  • NAYY
  • (N)AYY
  • RV-AI
  • XZ1(S) AI

Standards: IEC 60502.1 / IEC 60228 / HD603 / BS 5467/ BS 6724 / VDE0276-603

 

Medium-voltage cable

Copper

  • N2XS(F)2Y
  • N2XS(FL)2Y
  • (N)2XS(F)2Y
  • (N)2XS(FL)2Y
  • XLPE-PVC CU
  • XLPE-MDPE CU
  • XLPE-LSZH CU

Aluminium

  • NA2XS(F)2Y
  • NA2XS(FL)2Y
  • (N)A2XS(F)2Y
  • (N)A2XS(FL)2Y
  • XLPE LSZH Al

Standards: IEC 60502.2 / IEC 60228 / HD620 / BS 7870 / BS 7835 / BS 6622 / VDE 0276-620

 

Glass fibre and data cables

Standards: IEC 60794-1 / IEC 60793-2 / ISO/IEC 11801 / EN 50173-1

 

Cable glands and connectors

 

Protective cable systems, marking systems, accessories & tools

Solutions for solar parks

We are your one-stop shop for all the connections you need for your solar park, from cables to connectors.

Customised connection solutions

  1. Cost savings: Shorter installation time and reduction in labour costs
  2. Customised lengths and tailor-made connection solutions
  3. Customised markings possible with LAPP FLEXIMARK® marking systems
  4. Labelling of patches also possible on customer request (length, customer number, etc.)

Quality and security

We test all patches 100% at the end of production to ensure full functionality and the highest quality.

  1. Our ready-made garments are manufactured in Germany in LAPP factories under strict quality controls
  2. No faults: all connections are tested after production to ensure 100% fault-free products
  3. Additional connection certificates can be provided if required

Services

We do our best to provide you with the best possible support to make your project a success.

  1. Short-term and large-volume production possible for all lengths, even for large PV projects
  2. Direct delivery on site possible at the customer's request
  3. Customised packaging can be realised according to customer requirements

EPIC® solar connectors

Explore our extensive product portfolio for photovoltaic systems and find out more about EPIC® solar connectors.

Our customer references

Solar park in Estonia

LAPP has reliably supplied the Estonian company Energiapartner OÜ with EPIC® SOLAR connectors and solar cables since 2008, resulting in lower storage costs and delay-free projects. The durable solar cables and effective customer service were particularly appreciated.

Read now!

Solar park in Denmark

LAPP was awarded a major contract by European Energy for the construction of a 175MW solar park in Denmark, supplied 1,400 kilometres of solar cables and supported with distinctive project management to optimise deliveries.

Read now!

Photovoltaics on Turkish factories

General Solar used 500 kilometres of LAPP solar cable for a solar roofing project in Turkey. The high standard and European origin of the cables, as well as the efficient technical and logistical support provided by LAPP, cemented its position as the preferred supplier for future projects.

Read now!

Public Solar Park in Bundorf

LAPP ensures that everything runs smoothly by delivering solar cables for connecting to the power grid to the construction site just in time.

Read now!

Brainergy in Jülich

LAPP supplied solar cables, DC cables as well as fibre optic cables and AC medium-voltage cables. In addition to the proven quality, an important criterion for the contract was the delivery reliability.

Read now!

The biggest solar park in the Caribbean

The entire photovoltaic cabling, including string cables for connecting the modules, DC master cables for connecting to the inverters and fibre optic cables for data transmission, comes from LAPP.

Read now!

Photovoltaic system in Schönkirchen-Reyersdorf

With ÖLFLEX® CONNECT, fitters save time, and merely have to plug in and secure the cable. LAPP also impresses with its superior logistics. KPV Solar created a quantity framework for the project in its planning, and ordered it from LAPP.

Read now!

Solar Smart Grid in Haiti

LAPP provided a total of 45,700 metres of ÖLFLEX® SOLAR XLR cable to create a reliable connection between the individual photovoltaic modules. EPIC® SOLAR connectors were also used, among other things. PVC cables for direct burial and particularly resistant cable ties were also used.

Read now!

Solar park in South Korea

For such a large project, suppliers are required who can deliver the necessary components in large quantities and quantities in high quality on time. For the photovoltaic power plants, LAPP supplied the cable – a total of several million metres.

Read now!

On the safe side: standards for the solar industry

Standards provide guidelines for manufacturers, installers and inspectors to ensure that photovoltaic systems provide electricity safely, efficiently and reliably by complying with the quality and safety regulations. Solar solutions from LAPP meet these standards. An overview of the most important standards.

VDE (Association for Electrical, Electronic & Information Technologies)

VDE is a German association that develops standards and guidelines for electrical and electronic products. VDE standards cover different aspects of solar technology, including the safety, performance and installation of photovoltaic systems.

IEC (International Electrotechnical Commission)

This global non-profit committee is active in more than 170 countries, and develops international standards for electrical engineering, electronics and related technologies. The IEC standards for solar technology include guidelines for photovoltaic modules, inverters, power measurement, installation, safety and more.

BS (British Standards)

The national standardisation body in Great Britain was the first of its kind in the world. Its standards include guidelines for various aspects of solar technology, which are similar to the IEC standards, but can also contain specific requirements for the British market.

What special requirements do cables and wires need to meet in PV systems?

The growing system voltage due to increasingly modern PV systems requires equally more powerful cables and components. We at LAPP have been tackling this challenge for many years, and solve the tasks with innovative solutions. To meet the constantly arising challenges caused by system voltage increases, we develop high-quality cables and components with a long service life and extreme robustness as the products are constantly exposed to the wind and weather. Reliable performance requires exceptional weather resistance to heat, wind and frost – and rodent protection is recommended too. At the same time, modern PV systems can supply energy for several decades.

To exploit the full potential of the power supply, the relatively young industry is working on new technologies and applications such as organic photovoltaics (OPV). The photovoltaic industry’s requirements for cabling solutions range from large, robust cables for direct burial in power stations right through to sophisticated connection systems for flexible OPV modules.

All these requirements pose a major challenge – and we are able to offer successful solutions owing to our experience and expertise.

What should you bear in mind for your product selection?

High-quality products and easy assembly are crucial factors when it comes to selection. If one of the cables becomes brittle or malfunctions, it affects all the other cables from the same drum. Since new installations and removals can be very expensive in this case, investing in durable and high-quality material is worthwhile in the long term.

When purchasing a solar connector, please be aware of the following points:

  • Product selection: Use the EPIC® SOLAR 4Plus male connector and the EPIC® SOLAR 4Plus female connector made of high-quality, UV-resistant plastic.
  • Crimp connections which have been carried out in a regulation-compliant manner are the best connections between cables and connectors. They reliably transmit solar energy throughout the photovoltaic system’s entire service life – over decades. Our LAPP connector system has a crimp termination for cable cross-sections of up to 10 mm².
  • The TÜV certification and the tests in accordance with the standard DIN EN 62852 (relevant for connectors for DC voltage applications in photovoltaic systems) indicate quality.

Why use LAPP products for this solar energy?

We are constantly developing our products and services. Striving for the greatest possible durability, robustness and extreme flexibility is what drives us. Thanks to special sheath materials, LAPP solar cables are not only flame retardant and halogen-free, but also resistant to ozone and UV. Our solar cables and solar connectors can also withstand extreme weather conditions such as heat, wind and frost, making them perfect for use in your outdoor systems.

The products in a solar system are exposed to the sun for years. The transmission of energy and the high resistance heat up cables and connectors, while the constant alternation between warm and cold due to the sun’s rays and heating during operation causes cables and connectors to be come brittle.

A variety of inspections and performance tests have been carried out with our ÖLFLEX® cables, solar cables, SKINTOP® cable glands and EPIC® SOLAR connectors in close cooperation with customers, the TÜV and the North American UL approval institute. This enables us to guarantee our quality standard. Our products are suitable for use worldwide and, of course, RoHS-compliant.

Can't find the right solar product for your needs? Together, we can develop individual solutions, tailor-made for you. Our experts would be delighted to advise you.

Incidentally: expert knowledge is required not only when selecting the components used, but also for assembling and using the components correctly. We would be happy to support you on site here too.

Everything from a single source. With us as a partner. Our project business team will be happy to advise you on the planning and implementation of your PV systems.

Solar cables for PV systems

Harness the power of the sun – with our cable range for photovoltaic systems and DC applications.

Shop online now