Stop losing money: 5 common mistakes in cable harnessing cost you more than you think

LAPP-harnessing-solutions-typo3-slider-26-4

The cheapest option usually looks fine in the beginning. You compare quotes, align on specifications, and everything appears clear. On paper, the harness does exactly what it’s supposed to do. The difference only becomes visible later not during purchasing, but during installation, commissioning, or when a system is already expected to run.

1. Testing is treated as a final step

At first, everything looks correct. The harness meets specifications, connections are in place, and basic checks pass. The problems appear later. A connection behaves differently under load, a signal isn’t as stable as expected, or something that worked in isolation starts failing within the system. By that point, fixing it is no longer simple.

01-0426

2. Components come from everywhere

One supplier for cables, another for connectors, another for assembly. It works, until something doesn’t. When issues appear, it’s no longer clear where responsibility sits. Time is spent aligning between parties instead of solving the actual problem.

02-0426

3. Integration is left to the last moment

On paper, everything fits. Installation takes longer but then components don’t align as expected. Small mismatches turn into adjustments — and adjustments start to add up. What should have been straightforward becomes something that needs to be figured out on site.

03-0426

4. One missing part stops everything

A system is nearly complete and then it waits. Not because of complexity, but because a single component is delayed or unavailable. At that point, even a small dependency becomes a blocker.

04-0426

5. “We’ll do it in-house” seems efficient

At the beginning, it often is. Then the volume increases, variants grow, and changes start coming in. What used to be manageable starts taking time from engineering, from production, and from people who were meant to focus elsewhere. And slowly, it becomes a bottleneck.

 

The bottom line

Most harnessing issues don’t come from dramatic failures. Most harnessing issues don’t come from dramatic failures. They come from small things that only become visible once everything comes together, at a point when time is limited and changes are harder to absorb.

That’s where cost is really created.

05-0426

LAPP Harnessing Solutions

LAPP Harnessing Solutions supports these situations across the full process from design and sourcing to assembly and testing so that harnessing doesn’t become the part that slows everything else down.

Standard or customised harnessing solutions - we got you.

Connecting success: LAPP Harnessing Solutions Customer Stories

Harnessing Insights:


Let’s start a partnership – contact us!
Fields marked with an asterisk (*) are mandatory.
Please note that we do not accept orders through this form. For orders and order-related enquiries, please contact your usual LAPP representative or our customer service team.