Food and beverage

Main image

For the highest hygiene standards

Cables for the food and beverage industry

There are few industries which are quite as multifaceted and demanding in terms of the requirements they impose on their operating conditions as the field of food and beverage technology. The strict hygiene and cleanliness requirements which exist in the food processing industry naturally also apply to implemented electrical components. The most important requirement here is that germs and impurities must not form and come into contact with the goods. This is why cables for the food industry, as well as connectors and cable glands, must be able to meet the highest quality requirements.

What special requirements do cables and wires need to meet in the food and beverage industry?

The strict hygiene regulations for handling foodstuffs stipulate particularly complex requirements for electrical components. The cables and accessories used must withstand a wide range of chemical, thermal and mechanical loads and also function perfectly at all times in refrigerated and damp rooms. In food production, machinery and systems are even cleaned for around 30% of the day. Highly corrosive and aggressive cleaning agents and chemicals are sometimes used to kill as many germs as possible and to prevent impurities. Handling under extreme temperatures is another challenge in wet or refrigerated rooms and for heating processes. Cables for food production must therefore be resistant to chemical, thermal and mechanical stresses and must be certified in accordance with FDA, ECOLAB® or hygienic design. This is the only way they can be used in the plants and production areas.

The requirements of the food industry at a glance:

  • Resistant to aggressive cleaning agents
  • Resistant to bio-oils, fats, fruit and lactic acids
  • Temperature resistant
  • Waterproof
  • Rust-free

Our products for the food and beverage industry

As a long-standing partner in mechanical and plant engineering, LAPP offers an extensive range of standard and specialised products that meet the high demands of the food industrybecome. Our in-house laboratory and testing facilities are also an important source of support.

What should you keep in mind when making your product selection?

Three zones are defined in food and beverage production. Depending on the zone, the external influences vary in terms of mechanics or temperature. We can offer you the right cables and connection solutions for your machinery and systems for all zones – hygienic design zone, spray zone and non-product zone. The selection of suitable components and their proper and professional use have a direct impact on the safety of employees and the final product quality – and this is the trump card here too. Minimising downtimes, ensuring quality, protecting employees – these are priorities in all industrial sectors, but particularly in food production. This is because in the food and beverage industry, once the processing of perishable foodstuffs ceases, it leads to profit losses as well as high costs as a result of waste disposal and the need to restart production. At the same time, health is always at stake for consumers in this industry.

L3-kuvitus

Why use LAPP products for the food industry?

The food industry is one of LAPP's focal industries. We have extensive specialist knowledge in this field and offer a comprehensive range of standard products which meet the most stringent requirements. As cable and connection specialists, we also have an impressive range of sophisticated special solutions that were developed specifically for the food and beverage industry in our in-house laboratory and test facilities. We have gained a wealth of experience in our international laboratories over the years. Around 100 different cleaning agents and more than 700 other substances such as oils, greases and emulsions have already been tested in conjunction with our product materials.

We collaborate with many different partners throughout the food and beverage technology industry and are familiar with their specific requirements. Whether in dairy processing and dairy technology, meat and fish processing, baking and confectionery processing, in beverage bottling plants or packaging machines – LAPP is the expert solution partner for cable and connection technology and guarantees maximum functionality and safety with its reliable and proven branded products.

Benefits of LAPP connection solutions at a glance:

  • Temperature-resistant and heat-resistant cables
  • Use of hybrid cables
  • Corrosion-resistant
  • Hygienic Design compliant
  • FDA approval and certification according to EHEDG, ECOLAB®IPA clean room suitability
  • Development with due regard for adequate component protection classes

Can't find the right product for your needs? Together, we can develop individual solutions, tailor-made for you. Our experts would be delighted to advise you.

Incidentally, expert knowledge is required not only when selecting the components used, but also for assembling and using the components correctly. We would be happy to support you on site here too.


    EXPLORE OUR SOLUTIONS AND SERVICES