Connectors and power plugs

Main image

For reliable connections – even after many plug cycles

The benefits of our connectors are clear: they create detachable connections between a cable and a device, for example, and withstand hundreds of plug cycles. EPIC® industrial connectors are used for power supply as well as signal and data transmission in various industrial environments and support the cable in its tasks: they supply another piece of equipment with power, control the signal transmission and guarantee data exchange. We offer a variety of connector variants for a wide range of applications and with different ordering options. Receive individual parts, kits or customised assemblies.

What are the connections used for?

In the past, electrical connections were hard-wired, soldered, and then often not touched for a long time, this task is now adopted by connectors that can be disconnected and reconnected again thousands of times, always create a reliable contact. A connector is therefore the elementary component of a detachable, secure connection between two cables or for connecting a cable to a device or machine.

Which connectors are there at LAPP?

Overview of possible connections with connectors

Not all connectors are made equal. The shape defines the function. Below you will find an overview of our connector range; from there, you can navigate much more easily to the product of your choice.

Find out on the respective sub-pages how industrial connectors are structured, which connection technologies are suitable for assembly, which areas of application result from the respective product group and much more.

When to choose MENNEKES or RAUSCHER & STOECKLIN connectors?

MENNEKES
In industrial applications, in mining, in railway and transport companies, in ports, harbors, and shipyards, on campgrounds: in all of these situations and many more, it‘s imperative to safely and reliably distribute electric power in challenging or harsh conditions. MENNEKES is a world-leading manufacturer of pin and sleeve wiring devices, switched and interlocked receptacles, disconnect switches and power distribution products. You can rely on their innovative, robust, and high-performance products that withstand the toughest conditions in industries throughout the world.

RAUSCHER & STOECKLIN
In applications where industrial electrical connectors are used, safety, quality and reliability all take top priority. Whether in tunnel construction where extreme mechanical strength is required or railway applications where vibration-proof is of highest importance, RAUSCHER & STOECKLIN robust, and efficient industrial electrical connectors are always the right choice

An industrial connector is the final touch added at the end of a cable that supplies another piece of equipment with energy, controls it, reads signals or transmits data from a transmitter to a receiver. 

Connectors can be found in all industrial environments: in mechanical and plant engineering, in control cabinets and of course in outdoor applications. The different shapes, sizes and variants enable a wide range of applications. Whether you want to establish a connection from the field level to the control cabinet, the control system or machine-to-machine communication, LAPP is sure to find the right product including all the necessary all-round information.

The trend towards miniaturisation and performance compression is not only evident in the cable area, but is also reflected in the connectors. Ideally, new connectors should be all-rounders, take up less space in the application, be PROFINET-compliant and vibration-resistant, and have comprehensive screening for maximum electromagnetic compatibility. 

At LAPP, we are making every effort to tackle new challenges with you as a customer and to develop the perfect connector for your respective installation site.

Two that fit together like a pot and a lid: cables and connectors

Cables and connectors are simply in perfect symbiosis. This is what Oskar Lapp (1921-1987) thought when he founded the LAPP family company in 1959 and brought the first industrially produced ÖLFLEX® power and control cables with coloured cores to the market. Shortly afterwards, the first rectangular connectors from the EPIC® product brand appeared and rounded off the portfolio.

EPIC has always stood for "Environmentally Protected Industrial Connectors".

L2-Epic-logo

Explore our cable range:

Our EPIC® products also meet your individual requirements:

L2-connectors-EPIC

From loose to assembled – you have the choice!

Kits and sets for minimised ordering effort

Don't feel comfortable researching and then purchasing all the individual components required for manufacturing a connector? Do you therefore want to reduce your ordering effort and eliminate the risk of incorrect orders?

Understandable – you're not alone in this! Many customers prefer assembled connector sets with optimally coordinated components. 

That is why you will find our kits for rectangular, circular and solar connectors in each connector product group, consisting of a housing, insert, contacts and cable gland, for example.

The worry-free ÖLFLEX® CONNECT package

If you like keeping things really convenient, effective connection technology also means we can produce plug & play solutions for you. Suitable for immediate use and perfectly assembled. Either with products from the standard range or customised. Get to your desired cable including an overmoulded connector in just a few steps!

Request your desired product now via ÖLFLEX® CONNECT

Connector term definitions

In recent years, the wrong individuals have become involved in technical language relating to connectors. Things that are usually still easily understood in casual language and oral communication can often lead to misunderstandings in written communication. We're tidying up incorrect designations! 

When used correctly, the commonly used term plug actually only describes the male variant, but not the whole connector. A connection consists of a male part, known as the plug, and a female part, known as the socket.

In the interior of the connector, a distinction is made between the pin and the socket.

What should you consider when it comes to connectors?

General information

Connectors are pieces of equipment that must NOT be plugged in or disconnected when used as intended, i.e. under electrical voltage (or technically under load). When connecting or disconnecting a connector under load, sparks and (briefly) high temperatures result which could destroy the contact surface and lead to the total failure of the connector.

Connectors may only be connected or disconnected when there is no current and voltage.

Soiling levels 1-4

The soiling level is a numerical value and indicates the environment for which the connector has been developed and tested. Soiling level 3 is typical for industrial environments, while soiling level 2 is typical for households.

Soiling levels and their significance:

Soiling level 1

  • There is no soiling or only dry, non-conductive soiling. The soiling has no influence on the properties of the connector. 
  • Open, unprotected insulation in air-conditioned or clean, dry rooms.

Soiling level 2

  • Only non-conductive soiling occurs. Occasionally, however, temporary conductivity due to condensation must be expected.
  • Open, unprotected insulation in residential, retail and other commercial premises, fine mechanical workshops, laboratories, test areas, medical premises.

Soiling level 3

  • There is conductive soiling or dry, non-conductive soiling that becomes conductive because condensation is to be expected.
  • Open, unprotected insulation in rooms of industrial, commercial and agricultural plants, non-heated warehouses, workshops, boiler houses.

Soiling level 4

  • Contamination results in constant conductivity caused by conductive dust, rain or snow.
  • Open, unprotected insulation in maritime or mining applications

EPIC® connectors are generally designed for soiling level 3 and therefore have high safety reserves, even if the connector is wet or dirty inside. The high reliability of EPIC® results from high quality materials and manufacturing expertise.

Rated voltage in volts

The rated voltage is the voltage according to which connectors are rated. It indicates at which voltage a connector can be operated continuously and without impairing its performance. 

Dependencies:

  • The rated voltage depends on the defined soiling level. If a connector was tested for soiling level 1, the rated voltage given in the technical data is significantly higher than if it was tested for soiling level 2. 
  • The rated voltage depends on the insulating properties of the materials used and the creepage distance (the distance between contacts on a surface).
  • The rated voltage depends on the clearance (the distance between contacts through air). 
  • The rated voltage depends on the pole configuration, i.e. the number of contacts. The more contacts are installed in a connector, the lower the rated voltage.

Rated impulse voltage in volts

The rated impulse voltage is the maximum voltage that a connector can withstand briefly under defined conditions without breakdown or flashover. At this specified voltage, there are no breakdowns or flashovers in the connector.

Rated current in amperes

The rated current is the maximum current determined by the manufacturer that can flow continuously through all contacts of the connector without the upper temperature limit being exceeded. The rated current is specified at an ambient temperature of 40 C. It is determined for the largest conductor cross-section that can be connected to the connector.

The rated current depends on the size of the contacts in the connector. As the contact diameter increases, so does the current.

Contact

Contact layers made of high-grade materials are essential to ensure a secure electrical connection over the long term. The contacts are usually coated using galvanic processes. In order to achieve a durable coating, the following requirements are placed on the base material and its contact layers: LAPP primarily uses silver (Ag) and gold (Au) for surface coating. 

Silver has the highest electrical conductivity of all metals. The passivisation of the silver surface delays the formation of an oxide layer and reduces the insertion and pulling forces. A brownish to black oxide layer of silver sulphide (Ag2S) forms due to sulphur or substances containing sulphur in the ambient air. However, this layer can be broken during the plugging process or is broken at high currents, so the required electrical conductivity is maintained. 

Gold is the most resistant precious metal. The formation of oxides and sulphides can be ignored. Gold contacts are characterised by low insertion and pulling forces. They are mainly used for the transmission of signals with low current and voltage values. 

EPIC® products only use high-quality stainless metal alloys for coating the contacts.

When selecting a connector insert, the insert that can accommodate at least the number of contacts required for the connection must be selected. Connector inserts containing more contacts are also selected in the application. This means that the same connection system can often continue to be used when the application is expanded.

Plug cycles

Each time a connector is connected or disconnected, this represents one plug cycle.  If a connector is subjected to too many plug cycles, this will have negative effects on the contact resistance and also on the coating of the contact area. When determining the maximum number of plug cycles, a test is carried out to find out how many plugging and disconnecting actions cause the contact resistance to increase to an unacceptable level. It must not increase by more than 50% or exceed a maximum of 5 mOhm.

Owing to the high-precision manufacture of the contacts and the choice of contact materials, the EPIC® connector has a very long service life.

Electromagnetic compatibility

Electromagnetic compatibility, or EMC for short, is the ability of electrical equipment to function satisfactorily in its electromagnetic environment without impermissibly influencing the environment, which also includes other equipment, or being influenced by it (DIN/VDE 0870, Part 1). 

In industrial environments, the interference frequencies normally lie in the frequency range below 100 kHz. In this frequency range, the most important factor is low-impedance, large-scale, 360° screening. 

Connectors that are protected from electromagnetic interference have housings with a metallic, conductive surface, a good electrical connection to the mating component and are equipped with a cable gland that allows the cable shield to be electrically connected to the housing.

EMC plugs are mainly used in the area of circular connectors. For rectangular connectors, the EPIC® ULTRA housings have been specially developed to meet these requirements.

Find out more about EMC

Coding

Coding is an arrangement which prevents connectors which are identical other than their different polarisation from being mixed up, i.e. incorrect plugging and cabling. This is suitable if two or more identical connectors are attached to the same device.

Coding can be performed with a coding key or coding insert, or using coding pins that can be screwed into the housing. With EPIC®, there is a coding option optimised for every connector system, such as coding-capable inserts and housing, as well as pre-coded circular connectors.

Temperature range

The temperature range is determined by the upper and lower limit temperature. The limit temperatures are the maximum and minimum permissible temperatures at which a connector may be operated.

L2-connectors-photo